CAP#.STATE
Description
Reports if the capture channel has captured a value. When the first value is captured, this will change to one and stay at one. This is reset to zero when the capture is armed.
If capture is configured to auto-rearm, CAP#.REARM is 1, then this will be set to one on the first trigger but will not change on subsequent triggers. In this case, you may want to use CAP#.COUNT to detect when each new value has been captured.
Examples
Usage
0: Not Captured
1: Captured
Code
-->CAP1.STATE 0 -->
Context
See Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
CAP1.STATE |
4400h |
08h |
Unsigned8 |
- |
- |
Read only |
No |
|
CAP2.STATE |
4401h |
08h |
Unsigned8 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
31090 |
1 |
31090 (0x7972) |
CAP1.STATE |
Unsigned8 |
Read Only |
Yes |
|
31091 |
1 |
31091 (0x7973) |
CAP2.STATE |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CAP1.STATE |
31090 |
Unsigned8 |
Read Only |
- |
|
CAP2.STATE |
31091 |
Unsigned8 |
Read Only |
- |
Related Topics